NXOpen.UF.Ugmgr.EncodePartFilename¶
-
Ugmgr.
EncodePartFilename
()¶ Refer to UF_UGMGR_encode_part_filename for documentation.
Signature:
EncodePartFilename(partNumber, partRevision, partFileType, partFileName)
Parameters: - partNumber (str) – Part number.
- partRevision (str) – Part revision.
- partFileType (str) – Part file type. Should be NULL, the empty string “”, “master”, “specification” or “manifestation”. Note that “master”, “specification”, and “manifestation” must be spelt using lower-case letters only.
- partFileName (str) – Part file name. Only required if the part_file_type is “specification” or “manifestation”.
Returns: Encoded form of part file name. Declare this parameter with array size MAX_FSPEC_BUFSIZE.
Return type: list of str
License requirements: None