NXOpen.UF.Ugmgr.ConvertNameFromCli¶
-
Ugmgr.
ConvertNameFromCli
()¶ Refer to UF_UGMGR_convert_name_from_cli for documentation.
Signature:
ConvertNameFromCli(cliName)
Parameters: cliName (str) – Command Line Input format, e.g., “@DB/peters-part/A/spec/sheet1” Note: The separator used must not be a character which is already used in the part name, part revision, part file type or part file name. Valid separators are /@#$^&()|[]{}. Returns: Internal format “%UGMGR=3.2 PN=Peters-part -PRN=A...”. The caller must free this string by calling UF_free Return type: str License requirements: None