NXOpen.UF.Trns.CreateRotationMatrix¶
-
Trns.
CreateRotationMatrix
()¶ Refer to UF_TRNS_create_rotation_matrix for documentation.
Signature:
CreateRotationMatrix(origin, direction, degreesRotation)
Parameters: - origin (list of float) – Origin Of The Axis - Absolute Coordinates
- direction (list of float) – Direction Vector - Absolute Coordinates
- degreesRotation (float) – Rotation Angle In Degrees
Returns: A Tuple
Return type: A tuple consisting of (matrix,status)
matrix(list of float): Rotation Matrix. This must be declared to hold 12 doubles.
status(int): Status Code 0 - Success 1 - Direction Vector Is A Zero Vector
License requirements: None