NXOpen.UF.Trns.CreateCsysMappingMatrix¶
-
Trns.
CreateCsysMappingMatrix
()¶ Refer to UF_TRNS_create_csys_mapping_matrix for documentation.
Signature:
CreateCsysMappingMatrix(refCsys, destCsys)
Parameters: - refCsys (list of float) – Real Data For Reference Coordinate System rp1[0-2] is the origin in absolute coordinates. rp1[3-8] are the X and Y vectors in absolute coordinates.
- destCsys (list of float) – Real Data For Destination Coordinate System rp2[0-2] is the origin in absolute coordinates. rp2[3-8] are the X and Y vectors in absolute coordinates.
Returns: A Tuple
Return type: A tuple consisting of (matrix,status)
matrix(list of float): Resulting Matrix. This must be declared to hold 12 doubles.
status(int): Status Code 0 = Success 1 = rp1 Is Invalid 2 = rp2 Is Invalid
License requirements: None