NXOpen.UF.Tabnot.SectionPrefs Structure¶
NXOpen.UF.Tabnot.SectionPrefs is an alias for NXOpen.UF.TabnotSectionPrefs_Struct
-
class
NXOpen.UF.
TabnotSectionPrefs_Struct
¶ Bases:
object
Refer to UF_TABNOT_section_prefs_s for documentation.
Fields
NXOpen.UF.TabnotSectionPrefs_Struct.HeaderLocation |
Location to display header |
NXOpen.UF.TabnotSectionPrefs_Struct.MaxHeight |
The maximum height of the section. |
NXOpen.UF.TabnotSectionPrefs_Struct.OverflowDirection |
Direction to overflow sections |
NXOpen.UF.TabnotSectionPrefs_Struct.OverflowSpacing |
Distance to offset continuation sections (only used when table continues on the same sheet) |
NXOpen.UF.TabnotSectionPrefs_Struct.AttachPoint |
Point to which origin is attached |
NXOpen.UF.TabnotSectionPrefs_Struct.UseDoubleWidthBorder |
Should the border be double width? |
NXOpen.UF.TabnotSectionPrefs_Struct.BorderWidth |
Width of border if use_double_width_border is TRUE |
NXOpen.UF.TabnotSectionPrefs_Struct.DisplayContinuationNote |
Display continuation note flag |
NXOpen.UF.TabnotSectionPrefs_Struct.ContinuationNote |
Continuation note string |