NXOpen.UF.TabnotCellPrefs_Struct.Format |
Cell format |
NXOpen.UF.TabnotCellPrefs_Struct.Precision |
|
NXOpen.UF.TabnotCellPrefs_Struct.IsAFormula |
Does the formatted text get passed to the expression subsystem for evaluation |
NXOpen.UF.TabnotCellPrefs_Struct.ZeroDisplay |
The way that a numeric zero should display |
NXOpen.UF.TabnotCellPrefs_Struct.TextFont |
Index of NX font |
NXOpen.UF.TabnotCellPrefs_Struct.TextHeight |
Height of text in this cell |
NXOpen.UF.TabnotCellPrefs_Struct.TextAspectRatio |
Text aspect ratio |
NXOpen.UF.TabnotCellPrefs_Struct.Symbolaspectratio |
Symbol aspect ratio (only available in standard fonts) |
NXOpen.UF.TabnotCellPrefs_Struct.HorizJust |
Horizontal text justification |
NXOpen.UF.TabnotCellPrefs_Struct.VertJust |
Vertical text justification |
NXOpen.UF.TabnotCellPrefs_Struct.TextAngle |
Text angle in radians |
NXOpen.UF.TabnotCellPrefs_Struct.TextSlant |
Text slant angle |
NXOpen.UF.TabnotCellPrefs_Struct.IsVertical |
Is text displayed vertical? |
NXOpen.UF.TabnotCellPrefs_Struct.IsItalic |
Is text displayed italic? |
NXOpen.UF.TabnotCellPrefs_Struct.Strikethru |
Is text stricken thru? |
NXOpen.UF.TabnotCellPrefs_Struct.LineSpaceFactor |
Line space factor |
NXOpen.UF.TabnotCellPrefs_Struct.CharSpaceFactor |
Character space factor |
NXOpen.UF.TabnotCellPrefs_Struct.IsHidden |
Is display of text suppressed? |
NXOpen.UF.TabnotCellPrefs_Struct.TextColor |
Text color |
NXOpen.UF.TabnotCellPrefs_Struct.TextDensity |
Text density 1:Normal, 2:Heavy, 3:Thin, 0:Use Default |
NXOpen.UF.TabnotCellPrefs_Struct.BottomLineCfw |
Color/font/width of bottom line |
NXOpen.UF.TabnotCellPrefs_Struct.RightLineCfw |
Color/font/width of right line width follows 1:Normal, 2:Heavy, 3:Thin, 0:Use Default |
NXOpen.UF.TabnotCellPrefs_Struct.NmFitMethods |
Number of fit methods |
NXOpen.UF.TabnotCellPrefs_Struct.FitMethods |
Fit methods |
NXOpen.UF.TabnotCellPrefs_Struct.ReferencedSpreadsheet |
Referenced spreadsheet |
NXOpen.UF.TabnotCellPrefs_Struct.SsSheet |
Sheet referenced in spreadsheet |
NXOpen.UF.TabnotCellPrefs_Struct.SsRow |
Row referenced in spreadsheet |
NXOpen.UF.TabnotCellPrefs_Struct.SsCol |
Column referenced in spreadsheet |
NXOpen.UF.TabnotCellPrefs_Struct.Prefix |
|
NXOpen.UF.TabnotCellPrefs_Struct.Suffix |
|
NXOpen.UF.TabnotCellPrefs_Struct.FormulaSuffix |
This string gets appended to the cell text when the text is passed to the expression subsystem when evaluating the cell as a formula. |
NXOpen.UF.TabnotCellPrefs_Struct.Url |
|
NXOpen.UF.TabnotCellPrefs_Struct.IsProtected |
Is cell protected? |