NXOpen.UF.Subdiv.Isocline Structure¶
NXOpen.UF.Subdiv.Isocline is an alias for NXOpen.UF.SubdivIsocline_Struct
-
class
NXOpen.UF.
SubdivIsocline_Struct
¶ Bases:
object
Refer to UF_SUBDIV_isocline_s for documentation.
Fields
NXOpen.UF.SubdivIsocline_Struct.BodyTag |
The body to apply the feature to |
NXOpen.UF.SubdivIsocline_Struct.ExcludedFaces |
Array of excluded faces or NULL if not used The excluded faces are not considered when applying the feature. |
NXOpen.UF.SubdivIsocline_Struct.FaceCount |
Number of faces in the exclude array |
NXOpen.UF.SubdivIsocline_Struct.Direction |
SO direction to use for the isocline direction. |
NXOpen.UF.SubdivIsocline_Struct.AngleStr |
String value of the angle expression in degrees. |
NXOpen.UF.SubdivIsocline_Struct.SecondDirection |
Optional SO second direction to apply to the steep faces from the first direction. |