NXOpen.UF.Std.SetCgmSizeMode¶
-
Std.
SetCgmSizeMode
()¶ Refer to UF_STD_set_cgm_size_mode for documentation.
Deprecated since version NX5.0.
Signature:
SetCgmSizeMode(sizeMode, sizeValues)
Parameters: - sizeMode (int) – CGM Size Mode 1 = Scale 2 = Dimensions
- sizeValues (list of float) – Size Selection Array (2 element array) If size_mode=1, only size_values[0] is used for the scale of the CGM file, If size_mode=2, then size_values[0] is the X dimension of the CGM file, and size_values[1] is the Y dimension of the CGM file.
License requirements: None