NXOpen.UF.Std.CreateVrmlFile¶
-
Std.
CreateVrmlFile
()¶ Refer to UF_STD_create_vrml_file for documentation.
Signature:
CreateVrmlFile(fileName, tolerance, modeFlags)
Parameters: - fileName (str) – Name for the output VRML file.
- tolerance (float) – adjustment to facet tolerance. Values larger than 1.0 produce fewer output facets. Values less than 1.0 increase the number of facets generated.
- modeFlags (int) – Control bit fields for controlling output facets. The following are valid flags: UF_STD_OUTPUT_LIGHTS - output light sources when set. UF_STD_OUTPUT_MATERIALS - output material properties if set. UF_STD_OUTPUT_TEXTURES - output image textures if set. UF_STD_OUTPUT_BACKGROUND - output background/foreground information UF_STD_OUTPUT_VRML_2 - use VRML 2.0 specification if set.
License requirements: None