NXOpen.UF.So.SplineData Structure¶
NXOpen.UF.So.SplineData is an alias for NXOpen.UF.SoSplineData_Struct
-
class
NXOpen.UF.
SoSplineData_Struct
¶ Bases:
object
Refer to UF_SO_spline_data_s for documentation.
Fields
NXOpen.UF.SoSplineData_Struct.Method |
creation method:0 = through points 1 = from poles |
NXOpen.UF.SoSplineData_Struct.Degree |
degree of the spline curve |
NXOpen.UF.SoSplineData_Struct.Periodic |
0 = nonperiodic curve, 1 = periodic curve |
NXOpen.UF.SoSplineData_Struct.Nump |
number of positions (points or poles) |
NXOpen.UF.SoSplineData_Struct.Itype |
array of integers for interpolation type at each position: 0 = position only 1 = direction 2 = tangency (direction+magnitude) 3 = curvature (with tangency direction only) 4 = curvature (with tangency magnitude too) |
NXOpen.UF.SoSplineData_Struct.Position |
array of point ids for positions |
NXOpen.UF.SoSplineData_Struct.Parameter |
array of real values for point parameters |
NXOpen.UF.SoSplineData_Struct.Direction |
array of direction ids for tangent directions |
NXOpen.UF.SoSplineData_Struct.Magnitude |
array of scalar ids for tangent magnitudes |
NXOpen.UF.SoSplineData_Struct.Curvature |
array of offset ids for curvatures |
NXOpen.UF.SoSplineData_Struct.Symmetric |
symmetric option at start/end of the curve 0 = default 1 = symmetric model |