NXOpen.UF.So.OffsetSurfCvtrData Structure¶
NXOpen.UF.So.OffsetSurfCvtrData is an alias for NXOpen.UF.SoOffsetSurfCvtrData_Struct
-
class
NXOpen.UF.
SoOffsetSurfCvtrData_Struct
¶ Bases:
object
Refer to UF_SO_offset_surf_cvtr_data_s for documentation.
Fields
NXOpen.UF.SoOffsetSurfCvtrData_Struct.Face |
object id of the face which contains the evaluation surface |
NXOpen.UF.SoOffsetSurfCvtrData_Struct.Uv |
scalar object ids for the u and v parameters of the surface |
NXOpen.UF.SoOffsetSurfCvtrData_Struct.Option |
flag for evaluation option: 0 = u isoparametric 1 = v isoparametric 2 = section |
NXOpen.UF.SoOffsetSurfCvtrData_Struct.Secdir |
object id of the section direction |