NXOpen.UF.So.CreateXformThreePoints¶
-
So.
CreateXformThreePoints
()¶ Refer to UF_SO_create_xform_three_points for documentation.
Signature:
CreateXformThreePoints(objectInPart, updateOption, point0, point1, point2, scale)
Parameters: - objectInPart (Tag) – determines the context
- updateOption (
NXOpen.UF.So.UpdateOption
Refer to UF_SO_update_option_e for documentation.) – update option - point0 (Tag) – origin point
- point1 (Tag) – x-dir point
- point2 (Tag) – y-dir point NOTE: The y-dir specified as an input may be modified slightly if it doesn not result in a true orthogonal direction given the specified origin and x-dir.
- scale (Tag) – scalar ( NULL_TAG => IDENTITY )
Returns: Smart xform
Return type: License requirements: None