NXOpen.UF.So.CreateXformPntXyDirs¶
-
So.
CreateXformPntXyDirs
()¶ Refer to UF_SO_create_xform_pnt_xy_dirs for documentation.
Signature:
CreateXformPntXyDirs(objectInPart, updateOption, point, xDirection, yDirection, scale)
Parameters: - objectInPart (Tag) – Tag of object in part
- updateOption (
NXOpen.UF.So.UpdateOption
Refer to UF_SO_update_option_e for documentation.) – Update option - must be the same as the update option used to create the input point - point (Tag) – Tag of point
- xDirection (Tag) – Tag of x-direction
- yDirection (Tag) – Tag of y-direction
- scale (Tag) – Tag of scale value
Returns: Pointer to tag of smart transform
Return type: License requirements: None