NXOpen.UF.So.CreatePointAlongCurve¶
-
So.
CreatePointAlongCurve
()¶ Refer to UF_SO_create_point_along_curve for documentation.
Signature:
CreatePointAlongCurve(objectInPart, updateOption, curve, point1, t, option, flip)
Parameters: - objectInPart (Tag) – Tag of object in part
- updateOption (
NXOpen.UF.So.UpdateOption
Refer to UF_SO_update_option_e for documentation.) – Update option - curve (Tag) – Curve or edge
- point1 (Tag) – point
- t (Tag) – Scalar offset along curve
- option (
NXOpen.UF.So.PointAlongCurveOption
Refer to UF_SO_point_along_curve_option_e for documentation.) – Absolute/Relative offset option. Can be one of the following enumerated constants: UF_SO_point_along_curve_distance UF_SO_point_along_curve_percent - flip (bool) – If flip is set to TRUE, then t = -t
Returns: Pointer to tag of smart point
Return type: License requirements: None