NXOpen.UF.So.CreateDirrNormalToSurfacePoint¶
-
So.
CreateDirrNormalToSurfacePoint
()¶ Refer to UF_SO_create_dirr_normal_to_surface_point for documentation.
Signature:
CreateDirrNormalToSurfacePoint(objectInPart, updateOption, face, point, flip)
Parameters: - objectInPart (Tag) – Tag of object in part
- updateOption (
NXOpen.UF.So.UpdateOption
Refer to UF_SO_update_option_e for documentation.) – Update option - face (Tag) – Tag of the face.
- point (Tag) – Tag of the point on the face where the normal is to be created.
- flip (bool) – TRUE = Flip direction FALSE = Do not flip direction
Returns: Pointer to the tag of a smart direction.
Return type: License requirements: None