NXOpen.UF.Smd.SeqInput Structure¶
NXOpen.UF.Smd.SeqInput is an alias for NXOpen.UF.SmdSeqInput_Struct
-
class
NXOpen.UF.
SmdSeqInput_Struct
¶ Bases:
object
Refer to UF_SMD_seq_input_s for documentation.
Fields
NXOpen.UF.SmdSeqInput_Struct.ProcessAngle |
Process angle of the feature. |
NXOpen.UF.SmdSeqInput_Struct.Feature |
Feature on which the process is performed. |
NXOpen.UF.SmdSeqInput_Struct.ProcessName |
Name of the process in the forming table. |
NXOpen.UF.SmdSeqInput_Struct.ProcessType |
Type of the process in the forming table. |
NXOpen.UF.SmdSeqInput_Struct.Description |
Description of process in the forming table. |