NXOpen.UF.Sket.DimObject Structure¶
NXOpen.UF.Sket.DimObject is an alias for NXOpen.UF.SketDimObject_Struct
-
class
NXOpen.UF.
SketDimObject_Struct
¶ Bases:
object
Refer to UF_SKET_dim_object_s for documentation.
Fields
NXOpen.UF.SketDimObject_Struct.ObjectTag |
Tag of the object - sketch curves, edge, datum plane, datum axis, NX curves |
NXOpen.UF.SketDimObject_Struct.ObjectAssocType |
Object associativity type: UF_SKET_end_point; UF_SKET_arc_center - object must be an arc; UF_SKET_tangency - object must be an arc; UF_SKET_curve_point - object must be a spline UF_SKET_anchor_point - object must be a sketch conic |
NXOpen.UF.SketDimObject_Struct.ObjectAssocModValue |
Object associativity modifier: UF_SKET_first_end_point or UF_SKET_last_end_point if object_assoc_type = UF_SKET_end_point; Not Used if object_assoc_type = UF_SKET_arc_center or UF_SKET_anchor_point; parameter percentage (0 - 100) (used to find approx tgt pt) if object_assoc_type = UF_SKET_tangency; the index number of the defining point of the spline(starting from 1) if object_assoc_type = UF_SKET_curve_point; |