NXOpen.UF.Sim.AskAxisLimits¶
-
Sim.
AskAxisLimits
()¶ Refer to UF_SIM_ask_axis_limits for documentation.
Signature:
AskAxisLimits(engine, axis)
Parameters: - engine (PointerWrapper) –
- simulation engine object
- axis (str) –
- the name of the axis
Returns: A Tuple
Return type: A tuple consisting of (min,max)
min(float): - the minimum limit of the axis
max(float): - the maximum limit of the axis
License requirements: None
- engine (PointerWrapper) –