NXOpen.UF.Sfl.AskNthLoadDescriptorNx¶
-
Sfl.
AskNthLoadDescriptorNx
()¶ Refer to UF_SFL_ask_nth_load_descriptor_nx for documentation.
Signature:
AskNthLoadDescriptorNx(languageTag, index)
Parameters: - languageTag (Tag) – Language tag.
- index (int) – Index into list of load descriptors. Valid indices are from 0 to (number of load descriptors-1). The number of load descriptors can be obtained from function UF_SFL_ask_num_load_descriptors_nx.
Returns: The tag of the load descriptor.
Return type: License requirements: None