NXOpen.UF.Sf.MidsrfUserParms Structure¶
NXOpen.UF.Sf.MidsrfUserParms is an alias for NXOpen.UF.SfMidsrfUserParms_Struct
-
class
NXOpen.UF.
SfMidsrfUserParms_Struct
¶ Bases:
object
Refer to UF_SF_midsrf_user_parms_s for documentation.
Fields
NXOpen.UF.SfMidsrfUserParms_Struct.SolidBody |
Tag of the target solid body. |
NXOpen.UF.SfMidsrfUserParms_Struct.NumSheetBodies |
Number of sheet bodies. |
NXOpen.UF.SfMidsrfUserParms_Struct.SheetBodiesA |
Array of sheet body tags that will define the midsurface of the selected target solid body. |
NXOpen.UF.SfMidsrfUserParms_Struct.Thickness |
Thickness value to be used at formatting time whenever the automatic thickness extraction fails. |
NXOpen.UF.SfMidsrfUserParms_Struct.ConstThickness |
Constant thickness of all nodes of the midsurface. |