NXOpen.UF.Sf.SolutionAskSolverPropertyByIndexNx¶
-
Sf.
SolutionAskSolverPropertyByIndexNx
()¶ Refer to UF_SF_solution_ask_solver_property_by_index_nx for documentation.
Signature:
SolutionAskSolverPropertyByIndexNx(solution, property)
Parameters: - solution (Tag) – Tag for the solution.
- property (int) – Index into list of solver properties for the solution. Valid indices are from 0 to (number of solver properties-1). The number of solver properties can be obtained from function UF_SF_solution_ask_solver_property_count_nx.
Returns: Tag for the property.
Return type: License requirements: None