NXOpen.UF.Sf.PropertyAskValueNx¶
-
Sf.
PropertyAskValueNx
()¶ Refer to UF_SF_property_ask_value_nx for documentation.
Signature:
PropertyAskValueNx(propertyTag)
Parameters: propertyTag (Tag) – The tag of the property. Returns: A Tuple Return type: A tuple consisting of (boolValue,intValue,scalarValue,textValue,numLines,multiTextValue) boolValue(bool): Property value, if type SFOM_FEM_VALUE_BOOL.
intValue(int): Property value, if type is one of the following: UF_SF_FEM_VALUE_INT UF_SF_FEM_VALUE_ENUM
scalarValue(float): Property value, if type UF_SF_FEM_VALUE_SCALAR.
textValue(str): Property value, if type is UF_SF_FEM_VALUE_TEXT. NOTE: Caller must UF_free the string.
numLines(int): If type is UF_SF_FEM_VALUE_MULTI_STRING, this is the number of text lines in the property.
multiTextValue(list of str): If type is UF_SF_FEM_VALUE_MULTI_STRING, this is the array of text lines in the pr operty. NOTE: Call UF_free_string_array to free the storage allocated within the structure.
License requirements: None