NXOpen.UF.Sf.LocateStepLoadsNx¶
-
Sf.
LocateStepLoadsNx
()¶ Refer to UF_SF_locate_step_loads_nx for documentation.
Signature:
LocateStepLoadsNx(step)
Parameters: step (Tag) – Step tag. Returns: A Tuple Return type: A tuple consisting of (numMembers,membsPp) numMembers(int): Number of loads in the step.
membsPp(Tag): The pointer to the array of the tags of the loads. If num_members is zero, this pointer should not be used. If num_members is > 0, then this array must be freed by calling UF_free.
License requirements: None