NXOpen.UF.Sf.LocateSolutionLoadsNx¶
-
Sf.
LocateSolutionLoadsNx
()¶ Refer to UF_SF_locate_solution_loads_nx for documentation.
Signature:
LocateSolutionLoadsNx(solution)
Parameters: solution (Tag) – Tag of the solution. Returns: A Tuple Return type: A tuple consisting of (numMembers,membsPp) numMembers(int): Number of loads in the solution.
membsPp(Tag): The pointer to the array of the tags of the loads. If num_members is zero, this pointer should not be used. If num_members is > 0, then this array must be freed by calling UF_free.
License requirements: None