NXOpen.UF.Sf.LocateNodesOnMesh¶
-
Sf.
LocateNodesOnMesh
()¶ Refer to UF_SF_locate_nodes_on_mesh for documentation.
Signature:
LocateNodesOnMesh(meshTag)
Parameters: meshTag (Tag) – Mesh tag, pass in NULL_TAG to locate all nodes in current part. Returns: A Tuple Return type: A tuple consisting of (numOfNodes,nodeTagsP) numOfNodes(int): The number of nodes. Could be zero.
nodeTagsP(list of Tag): pointer to an array of node tags or NULL if the number of nodes is zero. This array must be freed by calling UF_free.
License requirements: None