NXOpen.UF.Sf.IsMidsrf¶
-
Sf.
IsMidsrf
()¶ Refer to UF_SF_is_midsrf for documentation.
Signature:
IsMidsrf(sheetBodyTag)
Parameters: sheetBodyTag (Tag) – Tag of given object Returns: A Tuple Return type: A tuple consisting of (isMidsrf,midsrfType,featureTag) isMidsrf(bool): Flag signifying the outcome: = TRUE –> object is a Midsurface = FALSE –> object is NOT a Midsurface
midsrfType(int): Tag of the midsurface feature if the object is associated with such a feature.
featureTag(Tag): Tag of the midsurface feature if the object is associated with such a feature. NOTE: If the midsurface is facepair type the feature of the facepair has as midsurface body the given sheet body.
License requirements: None