NXOpen.UF.Sf.EditLvNx¶
-
Sf.
EditLvNx
()¶ Refer to UF_SF_edit_lv_nx for documentation.
Signature:
EditLvNx(lvTag, lvName, scalingFactor, count, functionType)
Parameters: - lvTag (Tag) – Load Variation tag
- lvName (str) – The buffer must be declared using MAX_LINE_BUFSIZE so it can hold MAX_LINE_NCHARS characters. If NULL, value will not be modified.
- scalingFactor (float) – Scaling factor If NULL, value will not be modified.
- count (int) – Number of cycles If NULL, value will not be modified.
- functionType (
NXOpen.UF.Sf.LvFunctionMode
Refer to UF_SF_lv_function_mode_e for documentation.) – Scaling function type UF_SF_HALF_UNIT_CYCLE UF_SF_FULL_UNIT_CYCLE If NULL, value will not be modified.
License requirements: None