NXOpen.UF.Sf.EditDursolNx¶
-
Sf.
EditDursolNx
()¶ Refer to UF_SF_edit_dursol_nx for documentation.
Signature:
EditDursolNx(dursolTag, dursolName, stressCriterion, stressType, designLifeCriterion, fatigueCycles, kFactor, fatigueLifeCriterion, designCycles)
Parameters: - dursolTag (Tag) – Durability Solution tag.
- dursolName (str) – Name of Durability Solution. The buffer must be declared using MAX_LINE_BUFSIZE so it can hold MAX_LINE_NCHARS characters. If NULL, value will not be modified.
- stressCriterion (
NXOpen.UF.Sf.DursolStressCriterion
Refer to UF_SF_dursol_stress_criterion_t for documentation.) – Stress criterion If NULL, value will not be modified. - stressType (
NXOpen.UF.Sf.DursolStressType
Refer to UF_SF_dursol_stress_type_t for documentation.) – Stress type If NULL, value will not be modified. - designLifeCriterion (
NXOpen.UF.Sf.DursolDesignLifeCriterion
Refer to UF_SF_dursol_design_life_criterion_t for documentation.) – Design life criterion If NULL, value will not be modified. - fatigueCycles (int) – Number of fatigue duty cycles If NULL, value will not be modified.
- kFactor (float) – Fatigue strength factor (Kf) If NULL, value will not be modified.
- fatigueLifeCriterion (
NXOpen.UF.Sf.DursolFatigueLifeCriterion
Refer to UF_SF_dursol_fatigue_life_criterion_t for documentation.) – Fatigue life criterion If NULL, value will not be returned. - designCycles (int) – Number of design cycles desired for fatigue strength. If NULL, value will not be returned.
License requirements: None