NXOpen.UF.Sf.CreateSweptHexMesh¶
-
Sf.
CreateSweptHexMesh
()¶ Refer to UF_SF_create_swept_hex_mesh for documentation.
Signature:
CreateSweptHexMesh(solidBody, sourceFace, midnodes, elemSize)
Parameters: - solidBody (Tag) – The tag of the polygon solid body to mesh
- sourceFace (Tag) – The tag of the face to use as the source polygon face for sweeping.
- midnodes (bool) – If TRUE, Hex20s will be created. If FALSE, Hex8s will be created.
- elemSize (float) – Desired element size. This will be used to mesh the source polygon face and determine the number of sweeping layers.
Returns: The tag of the mesh created.
Return type: License requirements: None