NXOpen.UF.Sf.CreateSurfaceContactMesh¶
-
Sf.
CreateSurfaceContactMesh
()¶ Refer to UF_SF_create_surface_contact_mesh for documentation.
Signature:
CreateSurfaceContactMesh(sourceFace, targetFace, property)
Parameters: - sourceFace (Tag) – The source side polygon face on which contact need to be created.
- targetFace (Tag) – The target side polygon face on which contact need to be created.
- property (PointerWrapper) – Structure to define mesh properties. The valid structures are UF_SF_SURFACE_CONTACT_ANS_data_p_t, UF_SF_SURFACE_CONTACT_NAS_data_p_t, UF_SF_SURFACE_CONTACT_UGFEA_data_p_t
Returns: Pointer to the mesh recipe tag created.
Return type: License requirements: None