NXOpen.UF.Sf.AutoCreateMeshMatingCondition¶
-
Sf.
AutoCreateMeshMatingCondition
()¶ Refer to UF_SF_auto_create_mesh_mating_condition for documentation.
Signature:
AutoCreateMeshMatingCondition(entityNum, entityArray, mergeTolerance, makeMeshCoincident, coincidentFaceOnly, meshMatingType)
Parameters: - entityNum (int) – Number of entities in array
- entityArray (list of Tag) – Array of tags of the entities (polygon bodies)
- mergeTolerance (float) – Merge tolerance for assembly mesh
- makeMeshCoincident (int) – Make Mesh Coincident switch (0 or 1)
- coincidentFaceOnly (int) – Coincident face switch (0 or 1)
- meshMatingType (int) – Mesh mating type = 0 –> GLUE = 3 –> FREE NOTE: There is no 1 or 2 Type
Returns: A Tuple
Return type: A tuple consisting of (numAssemblyMeshes,assemblyMeshes)
numAssemblyMeshes(int): Number of assembly mesh tags created
assemblyMeshes(list of Tag): Array of assembly mesh tags created Free when done
License requirements: None