NXOpen.UF.Sf.AskStepNx¶
-
Sf.
AskStepNx
()¶ Refer to UF_SF_ask_step_nx for documentation.
Signature:
AskStepNx(lbcTag)
Parameters: lbcTag (Tag) – Tag of the load or boundary condition. Returns: A Tuple Return type: A tuple consisting of (numMembers,stepPp) numMembers(int): Number of loads and bc’s in the step.
stepPp(Tag): The pointer to the array of the tags of the steps. If num_members is zero, this pointer should not be used. If num_members is > 0, then this array must be freed by calling UF_free.
License requirements: None