NXOpen.UF.Sf.AskLvNx¶
-
Sf.
AskLvNx
()¶ Refer to UF_SF_ask_lv_nx for documentation.
Signature:
AskLvNx(lvTag)
Parameters: lvTag (Tag) – Load Variation tag Returns: A Tuple Return type: A tuple consisting of (lvName,scalingFactor,count,functionType,solutionStepTag) lvName(list of str): Name The buffer must be declared using MAX_LINE_BUFSIZE so it can hold MAX_LINE_NCHARS characters. If NULL, value will not be returned.
scalingFactor(float): Scaling factor If NULL, value will not be returned.
count(int): Number of cycles If NULL, value will not be returned.
functionType(
`NXOpen.UF.Sf.LvFunctionMode
Refer to UF_SF_lv_function_mode_e for documentation.`): Scaling function type UF_SF_HALF_UNIT_CYCLE UF_SF_FULL_UNIT_CYCLE If NULL, value will not be returned.solutionStepTag(Tag): Solution Step tag If NULL, value will not be returned.
License requirements: None