NXOpen.UF.Sf.AskIdealizeRegion¶
-
Sf.
AskIdealizeRegion
()¶ Refer to UF_SF_ask_idealize_region for documentation.
Signature:
AskIdealizeRegion(regionP, angleExp)
Parameters: - regionP (PointerWrapper) – Idealize region entity in which to query
- angleExp (Tag) – Expression used for the tagential edge angle which is used for the region boundary, Can be NULL_TAG
Returns: A Tuple
Return type: A tuple consisting of (seedFace,numBndFaces,bndFaces)
seedFace(Tag): Seed face for the region Pass NULL if return parameter is not wanted
numBndFaces(int): Number of boundary faces in the bnd_faces array. Can be 0 Pass NULL if return parameter is not wanted If NULL is passed in, bnd_faces will be returned as NULL
bndFaces(list of Tag): Array of boundary faces. Is NULL if num_bnd_faces == 0 Pass NULL if return parameter is not wanted
License requirements: None