NXOpen.UF.Sf.AskDursolNx¶
-
Sf.
AskDursolNx
()¶ Refer to UF_SF_ask_dursol_nx for documentation.
Signature:
AskDursolNx(dursolTag)
Parameters: dursolTag (Tag) – Durability Solution tag. Returns: A Tuple Return type: A tuple consisting of (dursolName,solutionTag,stressCriterion,stressType,designLifeCriterion,fatigueCycles,kFactor,fatigueLifeCriterion,designCycles) dursolName(list of str): Name of Durability Solution. The buffer must be declared using MAX_LINE_BUFSIZE so it can hold MAX_LINE_NCHARS characters. If NULL, value will not be returned.
solutionTag(Tag): Tag of the solution If NULL, value will not be returned.
stressCriterion(
`NXOpen.UF.Sf.DursolStressCriterion
Refer to UF_SF_dursol_stress_criterion_t for documentation.`): Stress criterion If NULL, value will not be returned.stressType(
`NXOpen.UF.Sf.DursolStressType
Refer to UF_SF_dursol_stress_type_t for documentation.`): Stress type If NULL, value will not be returned.designLifeCriterion(
`NXOpen.UF.Sf.DursolDesignLifeCriterion
Refer to UF_SF_dursol_design_life_criterion_t for documentation.`): Design life criterion If NULL, value will not be returned.fatigueCycles(int): Number of fatigue duty cycles If NULL, value will not be returned.
kFactor(float): Fatigue strength factor (Kf) If NULL, value will not be returned.
fatigueLifeCriterion(
`NXOpen.UF.Sf.DursolFatigueLifeCriterion
Refer to UF_SF_dursol_fatigue_life_criterion_t for documentation.`): Fatigue life criterion If NULL, value will not be returned.designCycles(int): Number of design cycles desired for fatigue strength. If NULL, value will not be returned.
License requirements: None