NXOpen.UF.Sf.AllocIdealizeRegion¶
-
Sf.
AllocIdealizeRegion
()¶ Refer to UF_SF_alloc_idealize_region for documentation.
Signature:
AllocIdealizeRegion(seedFace, numBndFaces, bndFaces, angleExp)
Parameters: - seedFace (Tag) – Seed face for the region (required)
- numBndFaces (int) – Number of boundary faces in the bnd_faces array. Can be 0
- bndFaces (list of Tag) – Array of boundary faces. Can be NULL if num_bnd_faces == 0
- angleExp (Tag) – Expression to be used for the tagential edge angle which is used for the region boundary, Can be NULL_TAG
Returns: Idealize region entity created Use UF_SF_free_idealize_region to free
Return type: PointerWrapper
License requirements: None