NXOpen.UF.Route.AskObjCornerInfo¶
-
Route.
AskObjCornerInfo
()¶ Refer to UF_ROUTE_ask_obj_corner_info for documentation.
Signature:
AskObjCornerInfo(objId)
Parameters: objId (Tag) – Object identifier to interrogate. Can be an RCP, a Bend Segment, or a Corner (Bend or Miter) object . Returns: A Tuple Return type: A tuple consisting of (crnTyp,crnRcp,crnObj,bool) crnTyp(int): Corner type such as UF_ROUTE_CORNER_NONE UF_ROUTE_CORNER_BEND UF_ROUTE_CORNER_MITER
crnRcp(Tag): Object Identifier of the RCP at this Corner only, else NULL_TAG
crnObj(Tag): Object Identifier of the Corner object. This is equal to obj_id if the input is a Corner. If the input is an RCP or Bend Segment this is the Corner object to that RCP or segment
retVar(bool): TRUE object is some kind of cornerFALSE otherwise.
License requirements: None