NXOpen.UF.Ps.ExportData¶
-
Ps.
ExportData
()¶ Refer to UF_PS_export_data for documentation.
Signature:
ExportData(bodyList, fileName)
Parameters: - bodyList (
NXOpen.UF.UF.List
Refer to ` <../ugopen_doc/uf/.html>`_ for documentation.) – List of bodies to be exported - fileName (str) – New File name to put output into. An error is generated if the file you specify already exists. If you specify a full pathname, then the Parasolid transmit file will be created there. If you specify a simple file name, the file will be created in the directory specified by the UGII_UGSOLIDS_TMP environment variable. If this environment variable is not defined, then the transmit file will placed in the /tmp, /var/tmp or TMP directory.
License requirements: None
- bodyList (