NXOpen.UF.ProcessAid.AskSourceObject¶
-
ProcessAid.
AskSourceObject
()¶ Refer to UF_PROCESS_AID_ask_source_object for documentation.
Signature:
AskSourceObject(objectArg, isRecurse)
Parameters: - objectArg (Tag) – linked/extracted object tag, whose source is to be retrieved
- isRecurse (bool) – FALSE if required just one level upinformation of the source TRUE if need to search the source recursively
Returns: A Tuple
Return type: A tuple consisting of (sourceObject,fileToOpen)
sourceObject(Tag): source object tag retrieved,NULL in case of any error
fileToOpen(str): file name, in case of opening error forthis file. NULL if we were able to get the source_object. This must be freed by calling UF_free.
License requirements: None