NXOpen.UF.ProcessAid.AskDatumObjects¶
-
ProcessAid.
AskDatumObjects
()¶ Refer to UF_PROCESS_AID_ask_datum_objects for documentation.
Signature:
AskDatumObjects(featureSet)
Parameters: featureSet (Tag) – tag of the datum location feature,datum point, certification point or measurement point feature Returns: A Tuple Return type: A tuple consisting of (numDatPoints,datumPoint,numDatVectors,datumVector,numSets,nObjectsInEachSet,objects) numDatPoints(int): number of datum points in the givenfeature set
datumPoint(list of Tag): object tags of the datum point in the given feature set. This must be freed using UF_free.
numDatVectors(int): number of datum vectors in the givenfeature set
datumVector(list of Tag): object tags of the datum vector in the given feature set. This must be freed using UF_free.
numSets(int): number of sets of objects
nObjectsInEachSet(list of int): number of objects in each set. Use UF_free to free this
objects(Tag): tags of the objects involved in thedatum feature. Use the function UF_free to free this
License requirements: None