NXOpen.UF.Point.CreateAlongCurve¶
-
Point.
CreateAlongCurve
()¶ Refer to UF_POINT_create_along_curve for documentation.
Signature:
CreateAlongCurve(curve, basePoint, t, option, flip)
Parameters: - curve (Tag) – object id of curve or edge
- basePoint (Tag) – object id of base point
- t (Tag) – object id of scalar offset along curve
- option (
NXOpen.UF.So.PointAlongCurveOption
Refer to UF_SO_point_along_curve_option_e for documentation.) – Absolute/Relative offset option.Can be one of the following enumerated constants: UF_SO_point_along_curve_distance UF_SO_point_along_curve_percent - flip (bool) – If flip is set to TRUE, then t = -t
Returns: object id of point feature
Return type: License requirements: None