NXOpen.UF.Plot.JobOptions Structure¶
NXOpen.UF.Plot.JobOptions is an alias for NXOpen.UF.PlotJobOptions_Struct
-
class
NXOpen.UF.
PlotJobOptions_Struct
¶ Bases:
object
Refer to UF_PLOT_job_options_s for documentation.
Fields
NXOpen.UF.PlotJobOptions_Struct.Colors |
Specifies colors used in plotting. |
NXOpen.UF.PlotJobOptions_Struct.UseDrawingSheetColors |
TRUE if custom colors associated with the drawing sheet are used in plotting the sheet. |
NXOpen.UF.PlotJobOptions_Struct.Widths |
Specifies widths used in plotting. |
NXOpen.UF.PlotJobOptions_Struct.UseDrawingSheetWidths |
TRUE if custom widths associated with the drawing sheet are used in plotting the sheet. |
NXOpen.UF.PlotJobOptions_Struct.Tolerance |
A unitless value that controls the accuracy or smoothness of plotted curve geometry. |