NXOpen.UF.Plot.SetUghpglTol¶
-
Plot.
SetUghpglTol
()¶ Refer to UF_PLOT_set_ughpgl_tol for documentation.
Signature:
SetUghpglTol(shiftTolerance, units)
Parameters: - shiftTolerance (float) – The amount of shift which will beallowed between two non-overlapping pair of vectors from the first and second plot file. If the vectors are within the shift amount, they are then considered one and the same.
- units (int) – Metric of English units.
License requirements: None