NXOpen.UF.Plot.SaveCgmForPlotLayout¶
-
Plot.
SaveCgmForPlotLayout
()¶ Refer to UF_PLOT_save_cgm_for_plot_layout for documentation.
Signature:
SaveCgmForPlotLayout(jobName, bannerOptions, cgmFileName)
Parameters: - jobName (str) – Name for the plot job
- bannerOptions (
NXOpen.UF.Plot.BannerOptions
Refer to UF_PLOT_banner_options_s for documentation.) – Specifies banner options.If NULL, current session banner options are used instead. If non-NULL, call UF_PLOT_ask_default_banner_options or UF_PLOT_ask_session_banner_options to initialize the structure before setting structure fields. Current session banner options are not modified by structure values. - cgmFileName (str) – CGM file name
License requirements: None