NXOpen.UF.Plot.SaveCgm¶
-
Plot.
SaveCgm
()¶ Refer to UF_PLOT_save_cgm for documentation.
Signature:
SaveCgm(drawingSheet, jobOptions, jobName, bannerOptions, cgmFileName)
Parameters: - drawingSheet (Tag) – The plot job represents thisdrawing sheet. If NULL_TAG, the plot job represents the current display image.
- jobOptions (
NXOpen.UF.Plot.JobOptions
Refer to UF_PLOT_job_options_s for documentation.) – Specifies plot job options.If NULL, current session job options are used instead. If non-NULL, call UF_PLOT_ask_default_job_options or UF_PLOT_ask_session_job_options to initialize the structure before setting structure fields. Current session job options are not modified by structure values. - jobName (str) – Name for the plot job
- bannerOptions (
NXOpen.UF.Plot.BannerOptions
Refer to UF_PLOT_banner_options_s for documentation.) – Specifies banner options.If NULL, current session banner options are used instead. If non-NULL, call UF_PLOT_ask_default_banner_options or UF_PLOT_ask_session_banner_options to initialize the structure before setting structure fields. Current session banner options are not modified by structure values. - cgmFileName (str) – CGM file name
License requirements: None