NXOpen.UF.Plot.PrintPlotLayout¶
-
Plot.
PrintPlotLayout
()¶ Refer to UF_PLOT_print_plot_layout for documentation.
Signature:
PrintPlotLayout(jobName, bannerOptions, printer, profile, numCopies)
Parameters: - jobName (str) – Name for the plot job
- bannerOptions (
NXOpen.UF.Plot.BannerOptions
Refer to UF_PLOT_banner_options_s for documentation.) – Specifies banner options.If NULL, current session banner options are used instead. If non-NULL, call UF_PLOT_ask_default_banner_options or UF_PLOT_ask_session_banner_options to initialize the structure before setting structure fields. Current session banner options are not modified by structure values. - printer (str) – Specifies the name of the printer onwhich the job is to be printed. If NULL, the default printer is used.
- profile (str) – Specifies the name of the desired profile for the printer. If NULL, the default profile is used.
- numCopies (int) – Number of copies to print.
License requirements: None