NXOpen.UF.Plot.PrintFile¶
-
Plot.
PrintFile
()¶ Refer to UF_PLOT_print_file for documentation.
Signature:
PrintFile(filename, printer, profile, numCopies)
Parameters: - filename (str) – Name of CGM or TIFF file to print
- printer (str) – Specifies the name of the printer on which the job is to be printed. If NULL, the default printer is used.
- profile (str) – Specifies the name of the desired profile for the printer. If NULL, the default profile is used.
- numCopies (int) – Number of copies to print.
License requirements: None