NXOpen.UF.Plot.AddJobToPlotLayout¶
-
Plot.
AddJobToPlotLayout
()¶ Refer to UF_PLOT_add_job_to_plot_layout for documentation.
Signature:
AddJobToPlotLayout(drawingSheet, jobOptions, jobName, units, origin, rotation, scale)
Parameters: - drawingSheet (Tag) – Tag of drawing sheet. If thisis NULL_TAG, the current display is being plotted.
- jobOptions (
NXOpen.UF.Plot.JobOptions
Refer to UF_PLOT_job_options_s for documentation.) – Specifies plot job options.If NULL, current session job options are used instead. If non-NULL, call UF_PLOT_ask_default_job_options or UF_PLOT_ask_session_job_options to initialize the structure before setting structure fields. Current session job options are not modified by structure values. - jobName (str) – Name of the job
- units (
NXOpen.UF.Plot.Units
Refer to UF_PLOT_units_e for documentation.) – Units used to define the plot originand extents. - origin (list of float) – The location of the plot originexpressed in the specified units.
- rotation (
NXOpen.UF.Plot.Rotation
Refer to UF_PLOT_rotation_e for documentation.) – Defines the orientation of theplot in the plot layout. - scale (float) – Defines the scale of the plot inthe plot layout.
Returns: If non-NULL the rectangular bounds ofthe plot in the layout (the coordinates of the lower-left and the upper-right corners of the plot in millimeters or inches as indicated by the units parameter) are returned.
Return type: NXOpen.UF.Plot.Extents
Refer to UF_PLOT_extents_s for documentation.License requirements: None