NXOpen.UF.Patt.CycleErrors¶
-
Patt.
CycleErrors
()¶ Refer to UF_PATT_cycle_errors for documentation.
Signature:
CycleErrors(ia1)
Parameters: ia1 (int) – On input the error found by the last call to this routine. If this routine has not been called yet, then set ia1 to 0 to start cycling. On output this will be the next error. The cycling is complete when a 0 is returned. Returns: A Tuple Return type: A tuple consisting of (ia1,cr2) ia1(int): Modified value of ia1
cr2(list of str): Part Name Where Error Occurred
License requirements: None