NXOpen.UF.Path.SpindleOn Structure¶
NXOpen.UF.Path.SpindleOn is an alias for NXOpen.UF.PathSpindleOn_Struct
-
class
NXOpen.UF.
PathSpindleOn_Struct
¶ Bases:
object
Refer to UF_PATH_spindle_on_s for documentation.
Fields
NXOpen.UF.PathSpindleOn_Struct.Speed |
is the speed of the spindle |
NXOpen.UF.PathSpindleOn_Struct.Maxrpm |
is the maximum allowed speed of the spindle |
NXOpen.UF.PathSpindleOn_Struct.Range |
the spindle speed range |
NXOpen.UF.PathSpindleOn_Struct.Mode |
|
NXOpen.UF.PathSpindleOn_Struct.Direction |
|
NXOpen.UF.PathSpindleOn_Struct.SpeedFlag |
the speed is output if and only if this flag is TRUE. |
NXOpen.UF.PathSpindleOn_Struct.MaxrpmFlag |
the maximum speed is output if and only if this flag is TRUE. |
NXOpen.UF.PathSpindleOn_Struct.RangeFlag |
the range is output if and only if this flag is TRUE. |